About Measurements

PathWave Vector Signal Analysis (89600 VSA) extends the traditional one measurement-at-a-time capability to multiple measurements-at-a-time. The "Multi-Measurement" feature provides simultaneous analysis of multi-standard, multi-format, or multi-carrier signals. Each individual measurement's data acquisition and signal processing are run concurrently. All individual measurement trace data results can be shown together "side-by-side" in a combined output. To learn more about Multi-Measurements, see Multi-Measurements Overview.

Multiple Measurements

The Measurements Dialog is used to create, run, and manage multiple measurements. If you are not familiar with 89600 VSA's multi-measurement capability, review the Multi-Measurements Overview topic. This topic provides valuable information that will help you to use the 89600 VSA multi-measurement features.

Click one of the following links for more information about configuring multiple measurements.

See Also

Multi-Measurements Overview

Measurements Dialog Box

Acquisition Styles

Use Cases for Multi-Measurement

Managing Multiple Measurements

TRIG OUT Measurement example